Industrial Automation Solutions

With robust R&D capability and solid industry experience for more than 20 years, Delta offers industrial automation products and solutions with superior quality, reliability and precision that find application in a broad range of industries, including electronics, components, photoelectric panels and food & beverages. We are dedicated to providing innovative and reliable smart, green manufacturing solutions for global customers, keeping our promise of “Automation for a Changing World”.

Services

CONTACT

Electronics

The quick turnover of electronic and IC devices accelerate development in the electronics industry. Manufacturers are facing severe competition, and the challenge of rising wages. This is why quick and efficient production with high quality is the key for the manufacturers. Automated production has become the optimized solution to save labor, and lower manual deviations for enhanced product quality and productivity.

Delta is dedicated to developing automation solutions that bring high-speed and precise manufacturing to production lines. To cater to market demands, Delta provides a broad range of automation products, such as AC motor drives, AC servo drives & motors, PLCs, machine vision systems, HMIs, temperature controllers and pressure sensors. Connected with high-speed fieldbus, Delta’s integrated solutions are applicable for transferring, inspection, and pick-and-place tasks. The precise, high-speed, and reliable performance effectively elevate product quality, and reduce defects for electronics manufacturers.

Electronics Solutions

  • PCB Drilling Machines
  • Wafer Inspection Machines
  • Visual Positioning for Chip Resistor Welding
  • 3D Glass Finishing Machines
  • Motor Winding Machines
  • Laser Soldering Production Line

Rubber and plastics

Rubber and plastics are common materials used in our daily lives as well as in national defense and aerospace technology to vehicles, machinery, electronics, and buildings. As the global green economy and eco-awareness are rising, new materials, technology and applications are accelerating the development and transformation of the rubber & plastics industry.

Delta is dedicated to the rubber and plastics industry contributing years of experience in power, electronics, and industrial automation. Delta offers a broad range of products, such as heavy-load AC motor drives, PLCs, HMIs, temperature controllers, power meters and industrial power supplies, an all-electric injection molding machine solution (including control panels, specific controllers, AC servo drives & motors, and temperature controllers) and a hybrid energy-saving injection molding solution (including control panels, specific controllers, AC servo drives & motors, oil pumps and temperature controllers). Delta’s wide range of offerings fulfill the requirement for energy-saving, precise, high-speed and efficient system control for the rubber and plastic equipment.

Rubber & Plastics Solutions

  • Injection Molding Machines
  • Rubber Calendaring Machines

Woodworking Machinery

Traditional furniture manufacturing and processing relies heavily on inefficient and inconsistent manual work. Equipped with only a simple processing function, traditional woodworking machinery requires different machines for complex processes, such as side milling and engraving. The monotonous processing makes it difficult to meet market demand, and the woodworking machinery industry is seeking a more advanced solution.

To meet application demands, Delta presents its latest motion control solution for woodworking machinery. With the EtherCAT and DMCNET fieldbus supported PC-based and CNC controllers, Delta’s advanced woodworking machinery solution can be widely applied to automated labeling machines, routers with automatic conveyor systems, PTP routers, 5-sided drilling and boring machines, machining centers for woodworking, solid wood door machines and mortise & tenon Machines.

Woodworking Machinery Solutions

  • Machining Center for Woodworking
  • Solid Wood Door Machines

Fluid Automation Systems

Fluid automation systems are mainly applied for controlling the complex processes of air-conditioning systems, air compressors, and water treatment plants. Replacing manual process management with an automated system achieves efficient and stable operations with distributed processing capabilities, constant control, and central monitoring.

Delta is dedicated in developing reliable and optimized automation products, such as PLCs, AC motor drives, servo drives and motors, HMIs, and temperature controllers. For high-end applications, Delta presents mid-range PLCs with excellent algorithms and stability. Adopting a modular design with various extension modules for system scalability, Delta’s mid-range PLC features integrated PLC programming software and an operation interface with multiple function blocks (FB). Delta also offers a variety of industrial Ethernet switches to connect different industrial networks for precise process monitoring. The highly efficient, stable, and reliable automation systems meet the requirements for a wide range of fluid system applications.

Fluid Automation System Solutions

  • Air Conditioning System
  • Air Compressors
  • Fluid Automation Systems

Logistics and Transportation

Manual work for parcel barcode scanning and sorting in the logistics industry is labor-intensive and inefficient. Delta’s automation solution for the logistics industry utilizes the linearity of lighting. As the lighting channels are shielded, the Communication Type Area Sensor AS Series detects the shielded position and quantity to calculate the dimensions and central point of the parcels, and transmits the data to the PLC for parcel distribution. Based on this data, the PLC commands the AC motor drive and servo systems to control the conveying speed and position.

Logistics and Transportation Solutions

  • Logistics and Transportation

Textiles

Delta offers an energy-saving, high-speed, automated and digitized solution for cotton spinning equipment. To fulfill industry demands for tension control, simultaneous control, and high-speed precision operation, Delta's solution adopts encoders for precise positioning, and AC motor drives and PG cards for motor driving with the PLC as master control. Users are able to set the parameters, control the temperature, and monitor the process via the HMI. The solution can be widely applied to mercerizing machines, dyeing machines, rinsing machines, jig dyeing machines, tentering machines, and printing machines.

Delta's Textile Vector Control Drive CT2000 Series features specific wall-through installation and fan-less design for robust protection against cottons, dust, pollution and instant voltage fluctuation under harsh environments. It is suitable for spinning frames and roving frames in the textile industry, and can also be applied for machine tools, ceramics and glass manufacturing.

Textile Solutions

  • Textiles

Machine Tools and Metal Processing

Machine tools are usually used for precise metal cutting for metal parts processing. They are widely used in industries such as automobiles, aerospace, national defense, machinery, molds, electronics, generators and more. Delta provides a high-performance general-purpose CNC controller conforming to the international standard ISO G Code, and it integrates with a customizable human machine interface (HMI) for easy operation. The CNC controller comes with Delta’s AC Servo Drive ASDA-A3 Series, PMSMs (Permanent-Magnet Synchronous Motor), and AC motor drives to achieve quick data transmission via DMCNET, precise control of the motor’s constant speed and torque, and precise positioning of the machine tool.

Delta continues to cooperate closely with industries to develop more advanced and industry-specific CNC solutions to help customers enhance their sufficiency and competitiveness in the market.

Machine Tools and Metal Processing Solutions

  • Standard Lathe
  • Engraving Machine
  • Gantry Milling Machine
  • Machining Center Machine
  • Conversational Grinding

Printing & Packaging

As manufacturing industries upgrade to smart and digitized production, the packaging and printing industries, which are closely related to consumer products, have also advanced with highly efficient and accurate production processes. Efficient and automated equipment is required as a substitute for conventional systems for high yield rates.

Delta has long been devoted to industrial control and has complete automated production lines for hardware and software products to deliver highly integrated packaging / printing solutions. Delta also provides a variety of motion controllers and solutions supporting the CODESYS platform, CANopen, EtherCAT and more to meet the needs of diverse applications and help customers build smart processing equipment with high efficiency, high flexibility, and high competitiveness.

Printing & Packaging Solutions

  • Printing
  • Package
Contact